9/26/2016 1:00 PM | |
Posts: 6 Rating: (0) |
hi mark here is the log file. I couldn't figure out what's the problem from the log I'm just learning the PCS7
best regards Attachmentcompilation log file.txt (188 Downloads) |
9/26/2016 1:36 PM | |
Posts: 6 Rating: (0) |
this is the THPO.log file AttachmentTHPOFile1.txt (163 Downloads) |
9/26/2016 1:40 PM | |
Posts: 567 Rating: (107) |
There are two ways: 1. Use the standard blocks for PCS 7 V8.x. These are the APL (Advanced Process Library) blocks. 2. Install the PCS 7 Standard Library for PCS 7 V7.x. You can find the installation files in the additional products folder of the installation DVD. But I think the best way is to use the APL blocks. For every block in PCS 7 V7.x Standard Library (e. g. Valve) there is also a block in APL. It looks like you are doing the PCS 7 getting started? Link to a PCS 7 Getting Started with APL: SIMATIC PCS 7 process control system Getting Started - Part 1 (V8.0 SP1 or higher with APL) SIMATIC Process Control System PCS 7 Getting Started - Part 2 (V8.0 SP1 or higher with APL) |
Last edited by: Ralfinio at: 9/26/2016 1:44:42 PM |
|
9/26/2016 2:15 PM | |
Posts: 6 Rating: (0) |
yes. I'm using getting started to learn PCS7 but for now I wanna know why I can't see icon blocks in graphic designer even when library v7.1 how can I fix this ? best regards |
9/26/2016 2:44 PM | |
Posts: 567 Rating: (107) |
Maybe the picture "@PCS7Typicals.pdl" is missing in your WinCC project. Did you install the PCS 7 Library v7 from the DVD? Here is a list with FAQs for this topic. Hope you will find a answer. |
9/26/2016 2:51 PM | |
Posts: 6 Rating: (0) |
yes. I've installed library v7 before but in the case file is missed where can I get it from? and where should I past that? |
Follow us on