3/23/2020 3:57 PM | |
Joined: 3/13/2019 Last visit: 9/14/2023 Posts: 24 Rating: (0) |
Hi. Long time on this post but I do have the same task in front of me. If client 1 is active on screen 1 Server shouldn't be able to control any objects on screen 1. Would it maybe be easier to add a new client instead of the server? Script is not my cup of tea. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/24/2020 09:39:05New subject after splitting |
|
3/24/2020 7:23 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi AutoGen_6529156, the APL offers the block "OpStation" to configuration of the local operator control permission clients and server. The block converts the enabled operations or locks for up to 16 individual permissions in the bit-coded Out output. A detailed description of the block OpStation can be found in the manual PCS 7 Advanced Process Library (V9.0 SP2) at the section OpStations - Configuration of the local operator authorization. With regards |
Follow us on