6/23/2021 2:18 PM | |
Joined: 5/12/2006 Last visit: 10/8/2024 Posts: 22399 Rating: (3017) |
simple use the GSD File for the old not supported im module |
This contribution was helpful to1 thankful Users |
6/23/2021 2:19 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi walter_g, it is not possible to project the successor. the successor usually has newer functions, so if you project them, the predecessor doesn´t know them. The other way normally works, to have a newer HW than projected. Anyway,...you can project the older IM151-1 with GSD-file, which can be downloaded here: PROFIBUS GSD files: ET 200Shope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
6/24/2021 4:18 PM | |
Joined: 7/5/2006 Last visit: 10/1/2024 Posts: 180 Rating: (4) |
Many many thanks. |
Follow us on