6/9/2009 11:22 AM | |
Posts: 261 Rating: (42) |
Dear all, We are having a MP377 (6AV66440AB012AX0) and WinCC flexible 2007 (6AV66130AA572CA5). The technical data sheet showing the compatibility in between these two. (http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6AV6644-0AB01-2AX0&caller=view). Now the image file of the supplied MP is 1.0.2.0. In Wincc flexible 2007 S/W we found the image file for MP377 is 1.0.0.0. Image file 1.0.2.0 is not available. Please help. With best regards ddg |
Last edited by: ddg at: 6/9/2009 12:30 PM |
|
6/10/2009 7:46 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hi, I guess you already tried Hardware Support Packages (HSP) for WinCC flexible 2007. If I am no wrong with this package you'll receive 1.0.1 image of MP377. I suggest you to contact with Siemens Office in your place... Best regards Hristo Mihalev |
6/10/2009 8:44 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello again, In all documents seems that MP377 is "compatible" with WinCC Flex 2007. Look also in Which Engineering Software can be used with which panels? (last update of this documents is made on 2009-02-13 ). Best regards Hristo MIhalev |
6/10/2009 8:47 AM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8629 Rating: (1147) |
Dear ddg, Please have a look at this link: http://support.automation.siemens.com/WW/view/en/27774824 Here you see, you can program MP377 using WinCC flexible 2007 standard Maybe, these links are useful: http://support.automation.siemens.com/WW/view/en/21742389 http://support.automation.siemens.com/WW/view/en/28735883 Best regards, Wizard |
Last edited by: Wizard at: 6/10/2009 8:48 AMOooops, just too late. ;-)) I will try to type faster next time. |
|
6/11/2009 12:03 PM | |
Posts: 261 Rating: (42) |
Thanks to all We solve the issue.Great help from forum. With best regards ddg |
Follow us on