2/1/2023 3:01 PM | |
Joined: 4/24/2019 Last visit: 9/19/2024 Posts: 2 Rating: (0) |
Hello there! If you select one specific warning message and click on "Go to" you will be redirected to the exact chart and block related to the warning. There is a probability that, when you changed the CPU, something went wrong with the addresses. When you remove an address area on the HW Config, the CFC editor automatically changes the address that were connected to the blocks to textual interconnections. Compare your hardware configuration and the address connection to those blocks with your previous project. What was the procedure you made to change the CPU from 414 to 416 in the PCS 7 project? How do you replace a CPU 41x with the CPU 410-5H Process Automation? |
Follow us on