2/16/2022 12:03 PM | |
Joined: 2/10/2015 Last visit: 4/30/2024 Posts: 30 Rating: (2) |
Hello, I need your help please. I'm using WinCC V7.5.2.0 as server/client Simatic Net V16, Step7 Prof V14 SP1 and option in WinCC for Opc Server are installed. The licence for me are ok (Simatic Net Sofnet Lean Basic, WinCC Server, WinCC RT, Simatic Sofnet-ie Lean/Basic/Power Pack, WinCC Connectivity Pack) The os is Windows Server 2016 Standart Station configurator: OPC Server then WinCC Appl and IE General In Service (local) OpcUaServerWinCC don't Run when i clic run i have this message: Windows could not start the Opc... service on Local Computer --> Error 0x80004005 Unspecified. I have a another WinCC Server with the same configuration, only it's a real PC not a VM and Opc Server Running and working realy wheel. Thanks for your help Adrien ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/16/2022 14:23:41New subject after splitting |
|
Follow us on