12/7/2009 2:26 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Ok, Í'm busy on recovering the automation system on a plant. I have some documentation about the CFC software. I see that they used a block that represents a SM module. For examplea analog input (8 channels). In the block are the following parameters: - Bo_CH_use 00 (to 07) = enables channels - BO_SIMon 00 (to 07) = simulation on - SIM_V_00 (to 07) = simulation value - V0HRange (to 7) = maximum range - V0LRange (to 7) = minimum range - V0 (to ) =output value There are some more parameters, but this will make it clear. Is this a custom build block? or is this available on the library? Thank you Best regards, Sandor |
Last edited by: Sandor-CRX at: 12/7/2009 4:52 PMIf I could help you, you can use the RATE button. Thank you. |
|
12/8/2009 9:22 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hello Phantom, I'm not able to scan the cfc prinout, so i made a paint drawing. Hope it helps.. edit: the name: Analog iput d should be Analog input d |
Last edited by: Sandor-CRX at: 12/8/2009 9:25 AMIf I could help you, you can use the RATE button. Thank you. |
|
12/9/2009 4:56 PM | |
Posts: 2661 Rating: (279)
|
I am not aware of this block in the libraries I used. Could be a custom block with 8 CH_AI's. Are there MODE parameters in the left and connected? Regards |
12/14/2009 9:50 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Sandor-CRX, seems to be and old PCS7 version: in PCS7 v4 drivers block was for modules type, from PCS7 v5 drivers blokc for single I/O channel Regards |
12/14/2009 8:00 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hey CBo, I think you are right, The PCS7 version that was used isv4.0. I wonder why they changed it.... It is handy to make one CFC were all inputs and outputs are listed from one ET200 module. Now I have to make in almost every CFC at least one driver block to connect my input/output. Especially if I have over 150 I/O... Thanks for the reply! Now I know that there are some blocks which I cannot find in the new version, but did existed. |
If I could help you, you can use the RATE button. Thank you. |
|
12/30/2009 1:55 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hello Hello, So every I/O from ET200M should be connected to a driver block (CH_AI, CH_AO etc.). This means that I need 1000 (fully equipped plant) of those driver blocks. What I did: - I created in the plant hierarchy a hierarchy folder: Template_IO - In there I created the following charts: TEMPLATE_AI, TEMPLATE_AO, TEMPLATE_DI and TEMPLATE_DO - In the TEMPLATE_AI, I inserted 8 CH_AI driver blocks - The same goes for the other templates - Next, I copied the templates to the hierarchy folder which uses ET200M. - I renamed the TEMPLATE_AI to a easy name. - From there, I connect all my inputs/outputs from my S7-400 master symbollist - Whenever I need a input or output, I interconnect this to my CFC chart with all the I/O's. It seems a little too much work. Is there an easier method? |
If I could help you, you can use the RATE button. Thank you. |
|
1/4/2010 2:11 PM | |
Posts: 183 Rating: (8) |
Hi Sandor-CRX; What PCS7 version are you using? |
1/5/2010 7:54 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
I am using version 7.1..... |
If I could help you, you can use the RATE button. Thank you. |
|
1/5/2010 11:18 AM | |
Posts: 183 Rating: (8) |
Why don't you use Import-Export Assistant to insert and configure the charts? |
Follow us on