8/11/2017 8:32 AM | |
Joined: 7/14/2016 Last visit: 9/12/2023 Posts: 387 Rating: (27) |
Hello all, I am using TIA 13 SP1 wincc professional. I directly installed this setup without v13 previously installed. After setup completed it shows error, I am not sure it is of license or any other. Attached is screenshot and logfiles. I open new project or existing project, all are compiling without error but simulation is not starting saying 'failed to start simulation'. There is no error in project or windows evenlog. Please suggest. I already installed this setup twice. Kbv. AttachmentLOG_FILES.zip (108 Downloads) |
Last edited by: Kbv at: 8/11/2017 8:33:27 AMDon't just think in terms of solutions... |
|
8/11/2017 2:25 PM | |
Joined: 7/14/2016 Last visit: 9/12/2023 Posts: 387 Rating: (27) |
Hello Christophd, Thanks for reply. You are right. There is another logfile for SQL installation error. Here it is attached. Kbv. AttachmentSummary.txt (137 Downloads) |
Don't just think in terms of solutions... |
|
8/16/2017 11:31 AM | |
Joined: 6/19/2017 Last visit: 6/4/2024 Posts: 8134 Rating: (165) |
New question published by sna8810_0s is split to a separate thread with the subject Uninstalled v14 and installed WinCC Pro v13Sp1 - After that get error: Failed to start simulation. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on