11/23/2021 3:31 PM | |
Joined: 11/2/2021 Last visit: 2/18/2022 Posts: 10 Rating: (0) |
Hi, has anyone been able to integrate a debian package (program.deb) into the image-build-process and would like to present an example? I am stuck trying to add a very simple debian file. And it just won't work. The Idea was from here: prebuilt-deb I also expect that I will need the dpkg-prebuilt.bbclass But after 10 builds or so i haven't gotten any further. Thanks for your help |
Last edited by: xyztornado999001; at: 11/23/2021 21:56:10 |
|
11/24/2021 11:09 AM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating: (43) |
Can you share your recipe or the error messages you get? Hard to help otherwise. |
11/26/2021 11:23 AM | |
Joined: 11/2/2021 Last visit: 2/18/2022 Posts: 10 Rating: (0) |
This is what happens at the end of the build process:
I used the directory prebuilt-deb so that anyone can try the same. After copying it to the recipes-app directory and adding the line to the image rule of the example image (I only removed node-red and tcf-agent and tested this setup beforehand / didn't want to re-add it just for this test)...
...I would then start the build process with the standard command ./kas-container build kas-iot2050-example.yml |
11/26/2021 3:55 PM | |
Joined: 11/2/2021 Last visit: 2/18/2022 Posts: 10 Rating: (0) |
Great, that did it!! Thank you. |
Follow us on