2/19/2022 12:36 PM | |
Joined: 5/13/2021 Last visit: 3/5/2022 Posts: 4 Rating: (0) |
Hi, Is it possible to downgrade the firmware after upgrading it as in the manual "IOT2050_How_To_Firmware_Update_V1.0"? On my SD card I have old image: BUILD_ID="V01.00.02-0-g437270f" VARIANT="IOT2050 Debian Example Image" Can I downgrade my IOT2050 again to use the old SD card image? The manual says that "After the firmware update it is not possible anymore to boot the following operating systems: Example Image V1.0.2" But my old SD card (BUILD_ID="V01.00.02-0-g437270f) starts with new IOT2050 firmware. So if the system starts with the old SD card, it means everything will work fine, or do I need to downgrade my firmware also to the old version? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/21/2022 11:41:38New subject after splitting |
|
Follow us on