3/17/2018 11:37 AM | |
Posts: 74 Rating: (1) |
Thanks I got it working. Another question: My faceplate is 130x60, but when I drag it in to my pdl the size is 50x50. Are there a way to get is to be 130x60? BR Raffe ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/20/2018 12:36:07 PMNew subject after splitting |
|
3/19/2018 2:43 PM | |
Joined: 8/12/2016 Last visit: 5/21/2024 Posts: 101 Rating: (3) |
I face that problem too. I don't know if there is a way for that. |
3/27/2018 10:19 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hello, The'basic image' of the Faceplate Admin type has the dimensions 70x70, a rectangle but only 50x50 If the scaling of the faceplate instance is set to'not proportional', then the described effect appears after saveing/opening. However, if you change the size of the rectangle to 70x70 and move it to position X=0 and position Y=0, the scaling works as desired. Alternatively you could change the basic image size of the faceplate admin type to the size of the rectangle. It is only important that there is any object in the Faceplate Admin type that has the same height and width of the base image and is at position X=0, Y=0. Regards |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on