1/3/2024 12:29 PM | |
Joined: 1/3/2024 Last visit: 1/3/2024 Posts: 1 Rating: (0) |
Is there any distance limitation between to devices on single segment for Profibus network? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/04/2024 08:10:17New subject after splitting |
|
1/3/2024 1:06 PM | |
Joined: 3/11/2019 Last visit: 6/6/2024 Posts: 1459 Rating: (263)
|
There are limitations to max lenght, as well as minimum lenght with dependencies to transfer speed and also cable types. It can also be calculated based on "Weighting factors". Limitations based on topology, cable type and weighting factors are shown in PROFIBUS manual as mentioned above several times. SIMATIC NET PROFIBUS Network Manual System Manualregards sancruz |
Feedback appreciated, please rate |
|
Follow us on