6/24/2013 10:15 AM | |
Joined: 10/13/2012 Last visit: 3/5/2024 Posts: 79 Rating:
|
hiEkalavya [snip] ... i have another small doubt Is there any problem in "heidenhain ae lb 382c reader or scale" ...? this is gantry machine , gantry1(XDD1)master gantry2(XDI1) slave , now not synchronization two gantry , 1, alarm no: 10655 : channel 1 synchronization of gantry group1 in progrees , after 5sec going to emergency i want to know wheather problem is "control card orheidenhain ae lb 382c reader"..? I have attached photos see that difference , why this much different ..? Regards samiraj
AttachmentXDD1 XDI1.pdf (207 Downloads) |
Last edited by: CS Moderator at: 6/24/2013 12:49 PMnew subject after splitting from /tf/WW/en/Posts/93314 |
|
6/24/2013 7:54 PM | |
Joined: 12/29/2011 Last visit: 8/9/2023 Posts: 39 Rating:
|
The alarm :300608- XTD1 drive 7speed controller at limit. It is saying the XTD1 servo motor/drive is trying to move but cannot. Probably the drive cannot physically move the distance required to align the two gantry axes. It is putting a lot of/too much skew into the gantry so the drive errors. This is probably due to the huge differences in the scale readings. Write down in a notebook the existing values in MD34080 and MD 34090 for all axes. This is incase it all goes wrong and you have to start all over again. First you will have to have the reference positions and readings for both axes on the gantry approx equal. Adjust the following Axis MD to achieve this. MD34080 $MA_REFP_MOVE_DIST (reference point distance) MD34090 $MA_REFP_MOVE_DIST_CORR (reference point offset/absolute offset) Then when they are approx equal adjust one slightly to align the gantry axes at a right angle to the Y axis. You also need to read the attachment to understand how gantry axes work on 840D before doing anything. all the best Mr_Al AttachmentGantry.pdf (201 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on