8/5/2016 8:00 AM | |
Posts: 101 Rating: (3) |
Hi. I do my first project in WinCC flexible for operator panel OP177B. I have to make a MPI connection between this panel and CPU. Here are screenshots of what I did WinCC Flexible: https://s32.postimg.org/ummk86j3p/Screenshot_3.png Step7 & NetPro: p.s. CPU doesn't have any connections in the table is that ok?
Attachment1-4 Screenshots.zip (61 Downloads) |
Last edited by: anonym53 at: 8/5/2016 8:01:06 AMLast edited by: anonym53 at: 8/5/2016 8:04:56 AMLast edited by: anonym53 at: 8/5/2016 8:05:10 AMLast edited by: anonym53 at: 8/5/2016 8:05:52 AMLast edited by: anonym53 at: 8/5/2016 8:47:13 AMLast edited by: anonym53 at: 8/5/2016 8:53:46 AM |
|
8/5/2016 8:23 AM | |
Posts: 101 Rating: (3) |
Or I have to remove a connection from the table of panel in NetPro and create a new one in the table of CPU? e.g., I create in the table of CPU: https://s31.postimg.org/xowz735zv/Screenshot_5.png and it automatically creates active partner in the table of panel:
Attachment5-6 Screenshots.zip (67 Downloads) |
Last edited by: anonym53 at: 8/5/2016 8:23:28 AMLast edited by: anonym53 at: 8/5/2016 8:24:40 AMLast edited by: anonym53 at: 8/5/2016 8:26:20 AMLast edited by: anonym53 at: 8/5/2016 8:50:54 AM |
|
8/5/2016 8:29 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello, Is OK should work, remember to enable MPI channel on OP177 |
8/5/2016 9:41 AM | |
Joined: 4/24/2006 Last visit: 8/8/2024 Posts: 8713 Rating: (1166)
|
Hello, Perhaps this link might help: And in attachment Best regards, Wizard Attachmentwinccflex.zip (73 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on