5/18/2021 9:57 PM | |
Joined: 7/19/2014 Last visit: 2/15/2024 Posts: 10 Rating: (0) |
IT IS NOT POSSIBLE TO MODIFY "NET *" VARIABLES IN WEB SERVER ONLY is posible Variable "M*" |
5/18/2021 9:59 PM | |
Joined: 7/19/2014 Last visit: 2/15/2024 Posts: 10 Rating: (0) |
This is the program. Not is posible "ADD VARIABLE" type BOOL "V0.2" |
5/19/2021 5:02 AM | |
Joined: 12/18/2014 Last visit: 5/5/2024 Posts: 32956 Rating: (4075)
|
It is possible to manipulate the NetI and NetAI operands with the web server. You just have to know how to do it. It depends on how these operands are parameterized. - If they are parameterized with "Read value from localvariable memory (VM)", then you cannot manipulate with NetI and NetAI. In this case you have to manipulate the VM memory. See screen video "VM memory test". - If they are parameterized with "Read value from remote device", then you can manipulate with NetI and NetAI. See screen video "NetI and NetAI test". The screen videos are attached.
AttachmentScreenvideos.zip (225 Downloads) |
This contribution was helpful to1 thankful Users |
5/19/2021 12:52 PM | |
Joined: 12/18/2014 Last visit: 5/5/2024 Posts: 32956 Rating: (4075)
|
Why do you quote me in spanish? |
Follow us on