1/16/2007 11:16 PM | |
Joined: 1/7/2006 Last visit: 7/3/2023 Posts: 2705 Rating:
|
Dear Sameer, Please update your COM Profibus to version V5.1.2.3 {V5.1 SP2 HF3} and consider that you have to update all the hotfixes seperately and in the right order. [:blush:] You may find Hotfix 3 for COM PROFIBUS V5.1 in the link. To be able to install Hotfix 3, COM PROFIBUS V5.1 + SP2 + HF2 must be installed. You will find the Setup with the extensions of Servicepack 1 and 2, as well as Hotfix 1 and 2, under entry ID 11932277[;)] Please also consider to read in the newest GSD-file in your COM PROFIBUS, because this GSD files are updated frequently. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on