3/23/2023 1:07 PM | |
Joined: 1/21/2013 Last visit: 4/26/2024 Posts: 2714 Rating: (440) |
Hi Anikare, The controller input area for the KP8 is 2 bytes in size. Byte 0 is for the 8 keys, byte 1 is for the I/O terminals on the X60 interface that are configured as inputs. The output area is 4 bytes. Byte 0 is for the red switch backlight, byte 1 for the green and byte 2 for the blue. Note that not all of the 8 possible combinations can be used, see the manual for details. Byte 3 is used for the I/O terminals on the X60 interface that are configured as outputs. Kind regards |
4/14/2023 9:36 AM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello Anikare there is also a library available: https://support.industry.siemens.com/cs/de/en/view/63482149 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on