1/24/2017 3:49 PM | |
Joined: 7/29/2014 Last visit: 9/4/2024 Posts: 43 Rating:
|
”The selected online target could not be reached”. Tried with TIA, ProSave and Pack&Go. The most honest reply was given by ProSave - simply "Could not establish a connection". TIA is telling me there's a problem when connecting to the device, so no OS update or Revert to Factory available. It lets me connect to it, as in "Go online", but, after online, clicking on OS update or Revert to Factory does nothing. If I try OS update or Revert without being online, it tries to connect and fails with a "connection problem". I managed to get the OS update through the USB stick, with the firmware unpacked from a Pack&Go, like here. But there's no Revert in that local OS update, and there's no Revert in the menu, or I haven't found it... Where could I find the "older" FW, before the last update? As a side-issue, the PLC, a 1215, is now also telling me it requires a new firmware (4.1 to 4.2), again, after yesterday was silent as a dead fish.Ain't gonna see that happening! Correction> Actually, it seems it already has 4.2, offline is 4.1, yet I can't use 4.2 in TIA 13. Need 14 for that... |
Last edited by: norenendur at: 1/24/2017 3:59:31 PM |
|
1/24/2017 4:45 PM | |
Joined: 4/24/2006 Last visit: 7/4/2025 Posts: 9024 Rating:
|
Hello, Perhaps you can better start a ServiceRequest Let us know the result. Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
1/24/2017 5:46 PM | |
Joined: 7/29/2014 Last visit: 9/4/2024 Posts: 43 Rating:
|
Support request sent. Will let you know when I get a reply. |
Follow us on