10/23/2014 4:38 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349)
|
thanks I cannot tell you the answer. I can offer suggestions. Try the exact same library and project in V12 SP1 with latest update and GSD. See if it behaves properly. Was this an upgraded project or a built from scratch V13 project? If it was V11 or V12, and then upgraded, I would suspect the internals of the project are corrupted and you have to recreate the project in V13. Luckily you can just drag and drop most everything to the new V13 project if that is indeed what you need to do. You can also send your project to Support Requestfor evaluation. It may be a known upgrade issue, or you may need new firmware in your WP231, or a different library revision, or even a slightly different communications configuration. Post your results. |
science guy |
|
10/24/2014 3:14 PM | |
Joined: 3/11/2007 Last visit: 4/14/2024 Posts: 226 Rating: (13) |
Other screeshot of a portion of the program. |
10/24/2014 3:49 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349) |
Is your DB set up as symbolic or absolute addressing? |
science guy |
|
Follow us on