8/19/2020 1:46 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
hello The "M42 - License MultiAxes Package for D425-x" option licenses all functions of the Motion Control technology package that require a license (such as positioning, synchronism, path interpolation and cam) on a D425-x controller. It is valid for unlimited axes on one controller. If you use option M42, you do not need option C01 additionally. This information can also be found in the PM21 catalog on page 2/69 in the description of option M42. Here is the link to the PM21 catalog: https://support.industry.siemens.com/cs/ww/en/view/109751885 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on