6/24/2011 2:51 PM | |
Posts: 28 Rating:
|
When you want to decrease the setpoint you have to keepdecreasingbutton pushed untilcounter returns to the maximum value previously overtaken. Is there any way to set the maximum number of impulses of a counter below its maximum value 999999 ? I appreciate your suggestions. Thanks. Attachmentvelocidad.zip (312 Downloads) |
This contribution was helpful to
1 thankful Users |
6/24/2011 4:14 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, Ihave adjusted your circuit to limit the counter. Regards, Marcjan Attachmentvelocidad_new.zip (725 Downloads) |
Last edited by: Marcjan at: 6/24/2011 9:41 PMlittle mistake in the counter setting, should be ok now Problem solved? |
|
This contribution was helpful to
1 thankful Users |
6/26/2011 7:50 PM | |
Posts: 28 Rating:
|
|
This contribution was helpful to
2 thankful Users |
7/9/2011 4:43 PM | |
Posts: 28 Rating:
|
Attachmentvelocidad.zip (344 Downloads) |
7/12/2011 2:54 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi, look at my solution of a comfort version of key inputs: Cursor key can only used as sort puls inputs, external key can usedas long holded key inputs and so the circuit can workas auto pulser if external key is on a longer time. The input range can set by parameters and over the mux and the amplifivers the input values can scaled od translated... For your application to output a range from 0 to 1000 (for analog output modul) this can used to define Gain = 10 and so you must not input 1000 steps - then the input range is 100 steps for the hole range 0..1000.... The cirkuit at the attachment isbuilded as a complete circuit and can reduced.... I don´t know if the Fi-key can hold and then the program get a longer puls or if the Fi-kes only put a short puls to the circuit - please test it. External key replase with F-keyand in the other case cursor key replace with F-key... DEMO_TasterEingabe_eines_Wertes_aus_einem_Bereich.zip Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
6/25/2018 3:20 AM | |
Posts: 1 Rating:
|
Here attached: Example to allow the user to adjust multiple setpoints with a maximum value, and navigate between multiple setpoint screens on the LOGO! TDE Text Display. F1 and F4 navigate screen to screen. F2 to Increase setpoint value F3 to Decrease setpoint value. I hope others find this useful. V AttachmentCounter HI Limit_Setpoint_Multiple.zip (315 Downloads) |
Last edited by: vangel at: 6/25/2018 3:21:57 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on