5/13/2016 12:47 PM | |
Joined: 11/7/2012 Last visit: 8/5/2020 Posts: 59 Rating: (2) |
Can you provide a link of downloading the SP7 firmware.Actually I've SP6 and SP9 version but not the SP7. So it's not able to upload or going online with the PLC. Plzz help ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/17/2016 1:13:57 PMNew subject after splitting |
|
5/14/2016 3:40 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello KKDA; You will only find links for SP8/SP9 (as a single package download) fro MicroWin 4.0 on the forum. STEP7 MicroWIN V4.0 SP8 and SP9 https://support.industry.siemens.com/cs/ww/en/view/58523240 I do not understand what is your requirement for an old SP 7. Service Packs are generally backwards compatible, so any enhancement of SP 7 is available in SP 9. If you have justified usage for that particular download, then open a Support Request (link at the top of the page) and discuss it with Siemens support technicians. Hope this helps, Daniel Chartier |
Follow us on