1/22/2016 2:59 PM | |
Posts: 4 Rating:
|
All, Is it possible to load a program from a TP170B (Mono 6AV6 545-0BB15-2AX0) onto a TP177B DP-6 MSTM (6AV6 642-0BC01-1AX1) and operate as per the original HMI. Thank you in advance for any assistance. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/22/2016 3:34:06 PMNew subject after splitting |
|
1/22/2016 5:58 PM | |
Joined: 3/28/2015 Last visit: 5/23/2023 Posts: 705 Rating:
|
Hello, It is not possible to load the program from the panel TP170B into the panel TP177B TP170B BLUE MODE STN-DISPLAYCONFIGURABLE WITH PROTOOL/LITE FROM VERSION V5.2+SP2 TP177B 6" DP BLUE MODECONFIGURABLE WITH WINCC FLEXIBLE 2005 If you have the original program,you should migrate the protool configuration file to WinCC Flexibe 2008 SP2
|
Eng.Mohamed Ibrahim |
|
1/22/2016 8:50 PM | |
Joined: 1/21/2013 Last visit: 4/21/2023 Posts: 4617 Rating:
|
Hello, mmmh this panel have two configuration kit also with WinccFlexible http://www.jc-electronics.nl/files/cms/files/125/name/technical-data-6av6545-0bb15-2ax0.pdf Ok he need a original project but maybe without Protool |
1/23/2016 10:52 AM | |
Joined: 3/28/2015 Last visit: 5/23/2023 Posts: 705 Rating:
|
Hello, Of course ,I agree with our Expert Ste39 1-If you have the original project (programmed by WinCC flexible) so change the device type and download the project to the new panel. 2-If the original project (programmed by Protool)so do the migration. 3-If you haven't the original project,so program the project from the starting or contact the designer to give you it. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
1 thankful Users |
Follow us on