1/17/2018 8:10 PM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928)
|
Hi, I assume you are using the AP library. In that case, you can open the properties of the block and go to the settings you want at a higher level. The parameters such as Gain have an authorization level you can set at 1 or 2 or 3. The level corresponds with the user authorization in WinCC. Default the level is set at 2 I believe, so increase it accordingly to have a higher authorization. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on