10/13/2022 8:58 AM | |
Joined: 12/18/2014 Last visit: 7/23/2024 Posts: 33400 Rating:
|
The statement of the User WWEE is correct, in the both files is "program" instead of "pragma". See the screenshots
|
10/14/2022 8:24 AM | |
Joined: 9/19/2018 Last visit: 6/28/2024 Posts: 384 Rating:
|
HTML programmingis NOT a feature of LOGO!. You can already use all LOGO! data with the 4 standard pages of the Webserver. You can generate HTML code with LWE to get a graphic view of LOGO! data. If need more features or you want to improve something, you are free to change/enhance the code. But then you can’t continue with LWE. And only a HTML expert should try this. |
10/14/2022 10:21 AM | |
Joined: 12/13/2014 Last visit: 7/20/2024 Posts: 144 Rating:
|
What an stupid excuse.Don't use it because we don't intended to use it. HTML is NOT programming language or some kind of feature. It's an standardized way to present documents (rendered web page is essentially an document). > You can generate HTML code with LWE to get a graphic view of LOGO! data. Generated HTML is flawed. For creating HTML pages LWE uses templates, provided by Siemens as part of LWE package. Every person installing LWE gets same kind of wrong usage of meta keywords. I made bug report to Siemens 1.5 years ago (with explanation and simple way to correct issue - changing "pragram" to "pragma"). Now it fixed with another nonsense ("program"). And finally we all read (official?) answer from Siemens, that " If need more features or you want to improve something, you are free to change/enhance the code." Make LWE opensource then. With complete API, how data can be transmitted to LOGO SD card via Ethernet connection, how to start and stop LOGO etc. If you can't to this, then please stop lying. I again finalize my critics with sentence - LOGO is an industrial grade product (and priced as such). It's not an Arduino for hobby use, every customer here expects more polished product for that higher price ("you get what you pay for"). Thanks for reading. |
11/4/2022 10:00 AM | |
Joined: 9/19/2018 Last visit: 6/28/2024 Posts: 384 Rating:
|
It seems this was a misunderstanding. We talked to development again. “pragma” is a standard keyword of HTML language; this keyword function is “Forbid the browser to retrieve the page content from the Cache of the local machine. Once the setting is set, the page cannot be retrieved from the cache again”. It’s planned to improve this in the next version of LWE. |
Follow us on