6/3/2011 10:03 AM | |
Joined: 2/28/2010 Last visit: 5/23/2024 Posts: 55 Rating:
|
Yoga thankyou for your quick response. Q1. Is the WinCC RT on the Server 1(main server) getting activated on the server when no clients are connected? The answer to your first Q is; Yes the main server is activating RT well with or without the clients connected. Q2. Are there any error messages displayed either when the RT is getting activated or after the activation in the alarm logging about time synchronisation problems or connectivity problems? The answer to your second Q is; Their are no messages displayed on RT but there are some errors in alarm logging; I have attached a zip file examine it, and tell me whether it has to do with the problem at hand. Q3is the lmhosts.sam file on the clients containing the correct entries for the main server? What is the access path to the imhost.sam file? AttachmentError in messages.zip (120 Downloads) |
6/3/2011 10:32 AM | |
Joined: 2/28/2010 Last visit: 5/23/2024 Posts: 55 Rating:
|
Thankyou Yoga, AttachmentDiagnose.zip (101 Downloads) |
Follow us on