5/9/2016 8:49 AM | |
Posts: 4 Rating: (0) |
Hi all! I have a similar system under development, but my problem is this: I need the setpoint to be pre-programmable in 5 positions, selection via a binary switch. I just can't see, how I can even make the preselect function? I'm quite sure, it's possible to do, but I just can't see it? Finvlogo
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/9/2016 12:32:58 PMNew subject after splitting |
|
5/9/2016 9:21 AM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32895 Rating: (4067)
|
Here a possible solution proposal. Can be used upstream from the Logo 0BA5.
AttachmentSwitching_setpoint_(0BA5).zip (204 Downloads) |
5/11/2016 7:50 AM | |
Posts: 4 Rating: (0) |
Hello again! Don't know, if anyone noticed, but there was a slight bug in the binary hop from "011" -> "100", it reversed the direction... :) Just fixed it, attached is the entire schematic to play with... Thanks again for the help, this has many uses at our factory! Finvlogo AttachmentMX32-40 ROTOR LIFT SEAMLESS v1.0.lsc.zip (190 Downloads) |
Last edited by: Finvlogo at: 5/11/2016 7:51:15 AM |
|
Follow us on