8/1/2022 1:28 PM | |
Joined: 2/7/2020 Last visit: 1/10/2024 Posts: 101 Rating: (0) |
Dear Expert, How may sq mm wire maximum, we can wire to 1. 6DL1193-6TP00-0DN0 2. 6DL1193-6TP00-0DH1 Regards, Zankkar |
8/5/2022 11:02 AM | |
Joined: 7/5/2013 Last visit: 5/24/2024 Posts: 3091 Rating: (505) |
Hello Zankkar, see SIMATIC ET 200SP HA ET 200SP HA Distributed I/O system > Cable cross-sections and ferrules. Without ferrule: 0.2 to 2.5 mm2 With ferrule: 0.14 to 1.5 mm2 Regards, Frink |
Pi is exactly three! |
|
8/6/2022 3:59 PM | |
Joined: 9/21/2012 Last visit: 5/25/2024 Posts: 3949 Rating: (446) |
This also depends on the Ferrule cripers. Some of them crimp a 0,75mm2 wire so that it doesn't fit. |
Follow us on