2/24/2009 12:20 PM | |
Posts: 17 Rating: (2) |
Dear All , I willing to connect more than 100 , less than 125 , profibus nodes on CP443-5 within distance on 250 meters from CPU. Basically all these MCC cubicals with profibus interface. I have gone through theattahched manual, section , 5.2 Charactristics of DP interface. It says Number of DP slaves can be operated = 125 , but not saying anything about repeaters. DO I NEED REPEATERS for this network ?? OR , What is the Maximum Number of Profibus nodes we can have on CP443-5 without repeaters ?? Attachment4435ex_e.pdf (214 Downloads) |
2/24/2009 2:12 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello I think this link would answer to your question: What should you watch out for when using the RS485 repeater in PROFIBUS bus systems? regards |
2/26/2009 11:28 AM | |
Posts: 124 Rating: (17) |
Hello NitinW |
This contribution was helpful to1 thankful Users |
Follow us on