6/24/2011 2:13 AM | |
Posts: 32 Rating:
|
Hello all i want to know if i can measure flow of liquid with LU probe ? and if yes what configuration it need? best regards |
6/24/2011 7:50 PM | |
Posts: 32 Rating:
|
In my project i only have LU probe and need to measure flow what is the accuracy of it when measuring flow exactly? |
7/4/2011 9:36 PM | |
Posts: 74 Rating:
|
Hello blowouter The ProbeLU will convert a level to a flow but must be used with a primary element such as a flume or a weir. A simple paper on this is here http://cursos.puc.cl/unimit_agl_014-1/almacen/1219763720_lgurovic_sec4_pos0.pdf You cannot directly determine flowrate using rate of fill or discharge using the ProbeLU. It does not have these algorithms installed. The MultiRanger200 or HydroRanger200 does. Cheers Toppie[ |:) |
7/13/2015 3:31 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
|
This contribution was helpful to
1 thankful Users |
9/29/2015 1:38 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by gobi@ is split to a separate thread with the subject Measure a velocity of flow with SITRANS. Best regards |
This contribution was helpful to
1 thankful Users |
Follow us on