6/1/2020 11:59 AM | |
Joined: 2/5/2013 Last visit: 5/21/2024 Posts: 320 Rating: (74) |
Seems issue with TIA V15.1 updates. The program which is downloaded in controller is with higher update of TIA 15.1 and you have lower updates installed on your PG/PC. From Online-interfaces and search for accessible nodes, then online&diagnostics.You will get information from which version of TIA program is downloaded but it does not contains any information regarding updates. Install latest updates of TIA V15.1 Updates for STEP 7 V15.1 and WinCC V15.1 Br, AmolG |
Last edited by: Jen_Moderator at: 06/02/2020 11:07:11Optimized links. Please rate it. |
|
6/17/2020 4:49 AM | |
Joined: 11/1/2019 Last visit: 12/27/2023 Posts: 7 Rating: (0) |
Hello. I have the same inf msg 0604:000951 when i open tia 15.1 project that was given to me for add some functionality. I using the latests tia portal15.1 Update 4. Would i have a problem when i try to download edited project in the PLC? |
Follow us on