2/19/2018 9:55 AM | |
Joined: 5/31/2016 Last visit: 4/17/2024 Posts: 12 Rating: (1) |
Yes. All packages were installed although the naming has changed in v15. |
2/19/2018 10:09 AM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981)
|
Hello, which devices are configured in the project? (Sinamics S120)?
Christoph |
2/19/2018 10:24 AM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981)
|
Hi, do you have a sample project with the error which you can upload here? Christoph |
2/19/2018 11:32 AM | |
Joined: 5/31/2016 Last visit: 4/17/2024 Posts: 12 Rating: (1) |
Sorry, the file is too large for the forum. |
Follow us on