4/23/2018 9:56 AM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Good Morning. I would like to know if is possible the migration of HMI TP277 (WinCC Flexible 2008) to new Confort Panels (TIA Portal Vx.x). I don´t want migrate the Simotion Project, only the HMI The problem is TP277 is an integrated project with Step7 V5.4SP4 and Simotion Scout v4.1.1.6. Simotion D435 (6AU1 435-0AA00-0AA1 V4.1) If I tried copy from Step7 and then I tried migrated with TIA Portal V.13SP1, I can´t because the following fault "The Scout TIA Portal is requeried to migrate the project" What is the procedure if is possible? I don´t know if I have to migrate the full project to extract the HMI I have read topic like this:
Convert my Simotin scout v4.3 project to TIA Portal
Thank you |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/23/2018 10:04 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, first you must copy the WinCC from Step7 , after that you select the .hmi file for the Migration, not the Step7 project file. https://support.industry.siemens.com/cs/ww/en/view/54695062 Regards Christoph |
Last edited by: ChristophD at: 4/23/2018 10:05:09 AM |
|
4/23/2018 10:29 AM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Hi Christoph Yes, I have done that, and I get the following fault The Scout TIA is required to migrate the project. TIA Portal, don´t have Simotion Driver if you don´t have integrated project, so I think this is the problem. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/23/2018 11:23 AM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Thank you Chirstop I can´t because the OEM, But I have create a new project. I have done the following. - Insert to my project a new TP277, setup the connection with Simotion and 4 tags - Copy from Step7 and save the project - Migrate from WinCC Flexible to WinCC Flexible 2008 SP3 - Try to migrate from WinCC Flexible 2008 SP to TIA Portal V13SP1 (Fault, attached the screenshot) Regards AttachmentHMISimotionWCF2008SP3.zip (70 Downloads) |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on