3/27/2022 8:04 AM | |
Joined: 4/10/2021 Last visit: 3/21/2024 Posts: 70 Rating: (6) |
Hi I have a question regard to above discussions. I have CPU S7-414-5H equipped with Flash EPROM. These CPUs are in redundant mode and working properly. NOW I want to modify some CFCs and download them to CPUs without switching to STOP mode. (download modified CFCs in RUN mode). My questions: 1) is it possible to download in Online mode with above my system config.(CPU414-5H redundant + Flash EPROM MC as memory. 2) if answer is YES , how exactly should I do it , because the plant is working and I can not STOP the CPUs. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: ALI_N23 at: 03/27/2022 08:06:02Last edited by: Jen_Moderator at: 03/28/2022 06:58:10New subject after splitting |
|
3/28/2022 11:13 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
Closed cause question posted twice. The second thread with the subject Online edit CFCs (download to S7400 CPU in RUN mode) is published within the conference Process Control Systems SIMATIC PCS 7. Jen_Moderator |
Follow us on