5/6/2012 4:29 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Hi, You will need an MPI card for PG which will be PCI compatible, also you will need just regular ethernet card on PG and last but not least - you will need a router. Router is for NATing required ports and making your PG accessible from internet. As an example card for you PG you can look here COMMUNICATION PROCESSOR CP 5611 A2 |
Best regards, |
|
This contribution was helpful to1 thankful Users |
5/6/2012 10:39 PM | |
Posts: 559 Rating: (87) |
Dear haris_usama, Well you can do onething as i also did the same. If you are going to access the data remotely from the particular single PC then, You can purchase Teamveiwer software & install it in both the PG & Remote PC. By this you can access the PG Very easily, Even you can monitor PLC Program also. |
This contribution was helpful to1 thankful Users |
4/5/2013 1:31 PM | |
Posts: 3037 Rating: (192)
|
Hello, Which ports are used by WinCC flexible? Tweety |
Follow us on