3/9/2018 9:48 AM | |
Joined: 8/21/2014 Last visit: 5/24/2024 Posts: 961 Rating: (13) |
New question published by Masru is split to a separate thread with the subject DCM 80 Communication. Best regards |
My Forum is the place to personalize your profile, |
|
3/11/2018 8:00 AM | |
Posts: 69 Rating: (4) |
Can reversal of rotation only be done through field reversal? If it is so, should we use external contactors to do the same? How it is done? |
3/11/2018 11:11 AM | |
Posts: 69 Rating: (4) |
At what speed motor will run in reverse direction when using 50470? |
Last edited by: Masru at: 3/11/2018 11:13:04 AM |
|
3/11/2018 11:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Between 50 - 600 RPM with MotP PB. |
3/11/2018 3:31 PM | |
Posts: 69 Rating: (4) |
So it should be a selector switch for CW and CCW rotation? What if I need a PB to jog in reverse direction for a speed of 30rpm? |
Follow us on