7/25/2013 10:29 AM | |
Posts: 6 Rating: (0) |
Hello Sandman, The "OP ressources" on the CPU is set to "1". The "Cyclic operation" option is activated well, in WinCC flexible.
|
7/25/2013 3:04 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi BrunoAnt, Have you tried to put 16 in OP-resources? |
7/30/2013 5:00 PM | |
Posts: 6 Rating: (0) |
So, if i understand, as the"Cyclic operation" option is activated in the 16 panels,i have to put 32 in "op-ressources"? |
7/30/2013 5:14 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Yes try and let us know |
9/11/2013 11:25 AM | |
Posts: 3037 Rating: (192)
|
Hello, Which PLC do you use? How many panel do you use on the bus? Tweety |
Follow us on