8/19/2013 9:32 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the User DShailendra
|
This contribution was helpful to1 thankful Users |
8/23/2013 8:45 AM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating: (1159)
|
Hello, Please have a look at the following link: WinCC flexible: Engineering with Recipes Using Integrated Functionalities See chapter 2.2.3 (Import and Export Recipes) Best regards, Wizard |
8/25/2013 11:23 AM | |
Joined: 6/18/2012 Last visit: 3/14/2023 Posts: 16 Rating: (1) |
I have got it sir Thanks a lot !!!!!!!! |
This contribution was helpful to1 thankful Users |
8/27/2013 9:09 AM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating: (1159)
|
Hello, Here is a link how to connect HMI panel to network: how do you integrate an HMI operator panel into a local network? (It is now even possible to store the Recipes on a PC directory, which is also located on the network) My advise is not to use the internal flash for storing recipes. You should use a memory card to store the recipes or via Ethernet store them on a shared directory on PC. Best regards, Wizard |
Follow us on