Industry Online Support
Technical Forum
5/2/2007 9:42 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, it is possible with the function Backup/Restore from a CF Card. -> In the manual of the device there you will find a description for this (or look into the attachment). But i think this are not really good, because if you use a Mobile Panel, the place from the CF-Card are not easily to reach. And you need for each project a own Card. The Best are you use only one project and with the function "Connction point recognition" you can selcet each area. (A description of this you will find it in the manual -> http://support.automation.siemens.com/WW/view/en/23748871) greetings, |
Follow us on