9/2/2024 11:51 AM | |
Joined: 3/14/2008 Last visit: 9/4/2024 Posts: 2094 Rating: (936)
|
Hi, Can you add some print screens. It's a bit difficult to understand the issue |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
9/2/2024 6:14 PM | |
Joined: 12/20/2019 Last visit: 9/4/2024 Posts: 63 Rating: (0) |
Hi thank you for your attention: I put in three pic which in order 1,2,3 .so that pic related to 1 show main chart that use in instance way and pic 2,3 is another chart that is in main chart (1). i have emphasized with put mouse on specific input that use two times in pic2,3. then it showed error that "you use input in multiple connection without connect it ,connect it" when i compiled . nevertheless, it was not showed any error when compiled in pcs7 v7.0 and it correctly works. Attachmenterror.zip (1 Downloads) |
Follow us on