7/2/2009 12:35 PM | |||
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hi, Yes, you are right about reinstalling of OS. But sometime this is the last decision that could helps. BTW here has the same issue like yours fro other member. If you ask him maybe he found how to solve it. Look at IE General dissapears from Component Configurator Regards Hristo Mihalev |
||
7/2/2009 3:46 PM | |
Posts: 3 Rating:
|
Hi everybody, support.automation@siemens.com said: "until SIMATIC NET Edition 2007 (V7.0) the installed Ethernet cards in a PC are detected as one group from SIMATIC Plug and Play Manager. That means if you change IP parameters from one Ethernet card you change characteristics from whole group. This affects the projected Ethernet card in Station Configuration Editor." "If you want to use additional Ethernet cards while using running configuration in Station Configuration Editor you have to use SIMATIC NET PC Software Edition 2008 (V7.1)." I will try it!! |
Follow us on