8/23/2017 9:39 AM | |
Posts: 5 Rating:
|
Hello Everyone May i roll up this case once more. I have access to the Webserver now, but I still don't know why it is addressable on localhost and not on the PLC IP adress (.11). Now I changed the network Settings of X1 to 192.168.1.10 / 255.255.255.0 so the two adapters are in different subnets, as suggested. Still there is only one network adapter listend in Windows. I remember, that there where two network cards when I startet the Nanobox PC for the first time. The PLC network adapter disappeared after configuring with Tia Portal. Can anyone clarify why this PLC network card is gone? This question is also related with my target to get the OPC communication running here. Thanks for your Help. Cheers, Chris |
Last edited by: chriz3dd at: 8/23/2017 9:40:47 AM |
|
Follow us on