Industry Online Support
Technical Forum
10/4/2014 10:21 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (7) |
Is there a way to measure the natural frequency of a complete motor - load system with S120 drive? |
10/5/2014 7:42 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
YES |
10/6/2014 8:58 AM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (7) |
With what procedure? |
10/8/2014 10:24 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
... you can do it with the measuring functions. For example bode plot ottheclosed loop speed controller. |
Follow us on