3/28/2024 9:50 AM | |
Joined: 3/28/2024 Last visit: 3/28/2024 Posts: 1 Rating: (0) |
Hi. We need help to integrate Keyence displacement sensor and Siemens PLC. We are using Keyence GT2 and it starts communicating with S7-1215 DC/DC/DC PLC through Profinet successfully. The problem/query was about the data format. when the sensor got in contact with metal part, it shows some readings on the amplifier display like the readings are (2.4567 etc). Now i want these values inside the input addresses of PLC like in my case the addresses are I (18-24). but i can not get the readings on RDREC DB . Which seems to me that their is addresses issue or could it be the data format. I am confused about this. Moreover i switched the index value from 37 to 38 etc to check for different values, also switch different data formats. Please help me if you can in this matter. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/28/2024 13:17:23New subject after splitting |
|
Follow us on