5/23/2022 11:08 AM | |
Joined: 4/20/2018 Last visit: 4/17/2023 Posts: 4 Rating: (0) |
If I need to linking data from instance db input, output or in/out to hmi with PLC Data Type - how to do it in practice without creating additional global DB or static instance DB rows and in addition to updating them? [EDIT: 25.5.2022] If the instance-DB input, output or in/out are defined with the PLC Data type, then when calling the FB the inputs, outputs or in/out do not appear separately. If I only need to connect one of the ten inputs, for example, how can I do that? [/EDIT] The easiest would be if I could link the entire instance-DB to the HMI Tag. ------------------------------------------------------------------------------------------ |
Last edited by: _hj_ at: 05/23/2022 11:13:32Last edited by: Jen_Moderator at: 05/23/2022 13:54:52New subject after splitting Last edited by: _hj_ at: 05/25/2022 06:39:42 |
|
Follow us on