Industry Online Support
Technical Forum
5/23/2013 6:25 PM | |
Joined: 11/23/2011 Last visit: 4/17/2024 Posts: 202 Rating: (32)
|
Hello everyone, there is released a new LOGO! application for house control with master-slave communication. http://support.automation.siemens.com/WW/view/en/64143308 The following functions can be controlled manually or automatically:
-Controlling further areas and functionalities of a house control via still unassigned inputs and outputs -Operation with buttons and LOGO! TD -Switching all lights on and off immediately via panic buttons -Presence simulation when absent -Monitoringroom temperature and controlling the heating through setpoint input -Time- and temperature-depended control of certain house functions Bestgreetings, KM_AS |
This contribution was helpful to5 thankful Users |
6/25/2013 10:16 AM | |
Joined: 11/23/2011 Last visit: 4/17/2024 Posts: 202 Rating: (32)
|
Hello Tomy Master, thank you! Here is an overview of all links for new LOGO! Sets: Building automation: http://support.automation.siemens.com/WW/view/en/64143308 http://support.automation.siemens.com/WW/view/en/68585344 http://support.automation.siemens.com/WW/view/en/68585346 Distance and Level Measurement: http://support.automation.siemens.com/WW/view/en/21689394 Easy and reliable detection of objects by means of optical proximity switches: http://support.automation.siemens.com/WW/view/en/23588559 Greetings, KM_AS |
Follow us on