9/27/2013 5:48 PM | |
Joined: 11/23/2011 Last visit: 9/30/2024 Posts: 202 Rating: (32)
|
Hello N.Vijay, maybe the information in the following FAQ will be an approach to solution: http://support.automation.siemens.com/WW/view/en/7302326 Greetings, KM_AS |
10/1/2013 9:19 AM | |
Posts: 461 Rating: (29) |
Load with memory card will load the code in mmc or else it would load in the cpu memory.. Regards, Nelliyan.G |
12/13/2013 9:54 AM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715)
|
Hello,
Yes, the program and hw config are deleted.
Normal mres clears markers, timers etc. when done with mmc in wrong PLCtype it clears mmc. [Quote] Is thisalso apply for MC? No memorycard can only be erased with Step7 command. How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)? Regards, Marcjan |
Last edited by: Marcjan at: 12/13/2013 9:55 AMProblem solved? |
|
This contribution was helpful to2 thankful Users |
Follow us on