7/9/2021 1:44 PM | |
Joined: 9/12/2020 Last visit: 4/29/2022 Posts: 23 Rating:
|
Do you think my CF card should have the boot software? |
7/9/2021 1:52 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Its difficult to comment (which is PPU), MLFB number signifies it is empty card. e.g. for PPU 270/271/290 turning application software with license CF card MLFB number is 6FC5835-1GY40-5YA0 |
Last edited by: PISCEAN 2010 at: 07/09/2021 13:58:19 |
|
7/10/2021 7:10 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Because of present COVID-19 pandemic issues, most of office staff is working from home. That is why in my previous post, I suggeseted you to raise support request so that you will get help on line quickly.
Please note, your system is 828D Basic & not 808d Advance. User or machine tool builder needs to set MD of axes configured. In configuration of MD, basically axis motor, encoder interfacing to power module hardware ports are defined so that NC/PCU understands the axis configuration. In axis MD setting all axes related data e.g. velocity, gains, softlimit, gear stages, no of encoders connected etc. etc. are defined. While writting/developing PLC logic, user/programmer needs to configure input/outputs of field elements & set NC/PLC interface signals via which all operational interlocks are set. It is prime responsibility of machine tool builder or PLC logic developer. All NC/application related logic/interlock is written/developed by NC controller (e.g. in your case turning related , in Siemens NC software)
In your case, i.e. MODE selection is operational via communication & setting of correct HMI, PLC, NC interface siganls so that interlocks as per machine logic requirement are set & it is machine tool builder/OEM/PLC developer responsbility. To understand setting of these & other important NC/PLC interfacing signals, machine data setting, hardware interfacing etc. etc., please refer below manuals SINUMERIK 828D PPU and components SINUMERIK 828D software and hardware SINUMERIK 828D NC variable and interface signals SINUMERIK 828D Turning and Milling HTH |
Last edited by: Jen_Moderator at: 07/13/2021 06:57:06Optimized links. |
|
7/12/2021 9:32 AM | |
Joined: 1/19/2008 Last visit: 8/13/2024 Posts: 989 Rating:
|
Hi, The part number for your card is for an empty card. You need to load the software Pee |
Follow us on