10/24/2019 6:54 AM | |
Posts: 7 Rating: (0) |
Yes, we configure datalog as Siemens described. See attached scrennshots. |
10/24/2019 6:57 AM | |
Posts: 7 Rating: (0) |
Second screenshot |
10/24/2019 6:59 AM | |
Joined: 12/18/2014 Last visit: 6/3/2024 Posts: 33142 Rating: (4095)
|
And what does the parameterization of the data log look like? |
10/24/2019 7:29 AM | |
Posts: 7 Rating: (0) |
On SD card created zero length file 203_0 without any data. |
10/24/2019 8:34 AM | |
Joined: 12/18/2014 Last visit: 6/3/2024 Posts: 33142 Rating: (4095)
|
@Scorp, to the time, as he make the second pso with the entries, wrote I my post. |
10/24/2019 8:45 AM | |
Joined: 12/18/2014 Last visit: 6/3/2024 Posts: 33142 Rating: (4095)
|
Not the first 512 entries, that's not right. The buffer for data logging has 1024 Bytes. Is a SD Card in the LOGO!, saved the LOGO! the first 512 Bytes in the buffer before the LOGO! saved the logged datas on the SD Card. See attachment. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 276.pdf (338 Downloads) |
Follow us on