1/7/2009 3:13 AM | |
Posts: 2 Rating: (0) |
Hi, all I have a problem with onlining to S5 CPU921 via AS511 and RS232-TTY cable. Following the introduction on this forum, I have added a DB15 to DB25 convertor and supplied +5v on pin 14,12. But it still can't work. I see a message on AS511 manual, it said "Siemens S5 PU protocol not supported on S5135U CPU921 /16-BIT CPU". Then how can I online to this PLC? Can someone help? Thanks and Best regards! Nickchen email: yongbing.chen@alcoa.com |
1/7/2009 8:10 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello nickchen, This Simatic S5 type are not supported by AS511 protocol. Why does the online mode not work with the S5-PC converter TTY - RS 232? (only 5V on pin14) regards |
1/8/2009 9:09 AM | |
Posts: 2 Rating: (0) |
Hi, Umencho Thanks for your reply. But there shouldexist a way to program and online tothis plc. Have someone had this experience? Please help me! |
1/8/2009 11:32 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello nickchen, Look at this also. Maybe will help you to make the right cable. How do you connect a PG 7xx? Try cable with +5,2V in pin14 and ground signal of the +5,2V to the same as the CPU. Other way is to ask Mr. Late . regards |
Follow us on